FANUC UK MACH Show 2016



FANUC UK is celebrating a successful MACH 2016 exhibition, recording over 500 visitors to its stand. FANUC UK would like to thank all its customers and visitors for their valuable time during the show.

The MACH show, the largest manufacturing exhibition in the UK, inspired visitors from across the country. During the 5 day exhibition, FANUC UK registered over 500 visitor enquiries on the stand securing significant machine orders for Robotics, ROBODRILLS and ROBOCUT equipment.

Throughout the event, FANUC’s latest range was showcased including RoboMachines, Robots and FA/CNC control systems, including the latest in NEW HMI technology from FANUC, 2 collaborative robots CR35 and CR7, cutting demonstrations on the ROBOCUT (Wire EDM machinery) and ROBODRILL products.

To complement the machinery range, FANUC also displayed a range of part and material handling applications using our internal in-house systems capability for producing integrated loading and unloading cells.

Additional highlights of the stand included:

  • Servo door technology on the ROBODRILL products to give the customers an optimised cycle time and reduced labour requirements
  • Live cutting demonstration showing the high torque spindle capability
  • Simple interfacing of Robots to ROBODRILL products using “FANUC’s Ethernet-Interface 2”
  • EDM attachment for the ROBOCUT machines for Spark erosion of holes up to Ø3mm
  • FANUC’s collaborative CR7 robot serving drinks in the hospitality area.
  • FANUC’s collaborative CR35 robot loading a Renishaw equator and simulating the feedback of machining offsets to the FANUC CNC control system

Tom Bouchier, managing director, FANUC said: “These are exciting times for FANUC UK as we have just un-veiled our 107,000 sqft, UK facility at Ansty Park Coventry. The facility shows our commitment and passion to robotics and automation within the UK market place, enabling us to grow and at the same time improve our customer experience. Completion is due by March 2017 and the entire UK team are looking forward to the next phase in FANUC UK’s development.”

FANUC UK would like to thank the following partners for supplying equipment and hosting FANUC products on its stands:

  • Renishaw UK for supplying an Equator and hosting a ROBODRILL - D21LiA5 - 24K
  • Marposs for hosting a ROBODRILL D21Mi5 – 10K
  • Nikon for hosting an LRMate200iD/30B Robot
  • Mills CNC for displaying an M20iA – 20M in a compact Automation loading cell
  • Metrology Direct for displaying an LRMate200iD/30B Robot on an inspection loading display
  • New Technology CADCAM for hosting a ROBODRILL D21MiA5-10K

Official numbers from the Show:

MACH Visitors: 21,853
Cross-over: 3,774

Total: 25,627

See the fair video