ZAP-Mechanika

FANUC Provides Vision of the Future at ZAP

While machining can benefit greatly from the adoption of a machine-tending robot, the addition of 3D cameras introduces an extra level of intelligence that leads to autonomous production and particular benefits for manufacturers.
Case study video ZAP from FANUC Poland about electronics

Key Insights from Task to Result

Task

When an international manufacturer serving the electrical industry asked ZAP-Mechanika to machine a new design of clamping tool forging, there was a clear need for a fully automated production cell that would ensure a constant, defined cycle time.

Solution

ZAP-Mechanika asked sister company ZAP-Robotyka to design and create the automated machining cell. The cell features two FANUC ROBODRILL machining centres served by a single FANUC six-axis industrial robot equipped with two FANUC đť‘–RVision 3D vision systems.

Result

With their large field of vision, the FANUC 3DV/1600 3D vision sensors housed in đť‘–RVision systems recognise and pick up randomly located workpieces directly from a large tote bin. The robot subsequently loads and unloads parts from the two ROBODRILL machines. Notably, the vision-enabled cell also allows ZAP-Mechanika to work autonomously. The company can therefore produce two different components in a single cell, significantly accelerating the machining process with fewer resources.

ZAP-Mechanika

Established in 2000, ZAP-Mechanika operates a 173-employee, 5,800 m2 manufacturing plant in OstrĂłw Wielkopolski, Poland. Serving major brands from North America, Europe and Asia, the company is a leading manufacturer of mobile hydraulics and clamping tools. As an expert in precision metalworking, services at ZAP-Mechanika include component machining, heat treatment, precision measurement and metallurgy. A particular strength of this company is its close co-operation with customers at an early project stage to help develop the optimal machining process.

FIND OUT MORE ABOUT ZAP-Mechanika
Success story FANUC Poland - ZAP-Mechanika Headquaters

Two Different Components Produced in a Single Cell

“In our latest project for an international manufacturer of clamping tools operating in the electrical industry, we were tasked with creating a fully automated production line that would ensure a constant, defined cycle time for machining the clamping tool forgings,” explains Krystian Młynarczyk, Technologist at ZAP-Mechanika. ZAP-Mechanika subsequently engaged the services of sister company ZAP-Robotyka, an experienced specialist in the development and integration of robotic and automated workstations. Also based in Ostrów Wielkopolski, ZAP-Robotyka accepted the challenge, designing, constructing, delivering and implementing the entire production cell on behalf of ZAP-Mechanika.

Paweł Wróbel, Project Specialist at ZAP-Robotyka, explains the design and configuration: “In the robotic cell there’s a FANUC M-20𝑖D/35 six-axis industrial robot equipped with two FANUC 𝑖RVision 3D vision systems. The vision-enabled robot serves two ROBODRILL machining centres [𝛼-D21L𝑖A5 and 𝛼-D21L𝑖B5 models]. Each 𝑖RVision system connects directly to the robot, so ZAP-Mechanika can take advantage of extremely fast communication.”

Case study about successful implementation of FANUC Robodrill (machining centers) and a FANUC robot M-20iD/35 equipped with two FANUC đť‘–RVision 3D vision systems, at the Polish company ZAP Mechanika.

Thanks to the large field of vision, FANUC đť‘–RVision systems are able to recognise and pick up randomly positioned objects straight from a workpiece tote bin as large as a pallet. The robot subsequently loads and unloads parts to and from the ROBODRILL machines. But that is not all, there is an extra innovation in the cell designed by ZAP-Robotyka.

“The system allows ZAP-Mechanika to work autonomously,” reveals Marta Portasiak, Constructor at ZAP-Robotyka. “This non-standard approach makes it possible to produce two different components in a single cell, with a single robot, significantly accelerating the production process.”

The project also saw ZAP-Robotyka develop a novel system for gripping and manipulating parts, and design special tooling for the workstation.

Case study about successful implementation of FANUC Robodrill (machining centers) and a FANUC robot M-20iD/35 equipped with two FANUC đť‘–RVision 3D vision systems, at the Polish company ZAP Mechanika.

“The application has increased our productivity with fewer resources, while making our work easier and delivering continuity across the process,” says Tomasz Krazynski, CEO at ZAP-Mechanika.

A traditional set-up to machine the clamping tool forgings would require three machine tools and three operators. In contrast, ZAP-Mechanika is using only one operator, one FANUC robot, two FANUC machine tools and two FANUC 3D cameras.

“This cell clearly sets out our goals for the future,” concludes Krazynski. “We’ll continue to invest in automation moving forward and keep developing robotic production cells.”

Get Inspired

FANUC Success with Robots, ROBOSHOT and ROBODRILL - Erkul Cosmetics in Turkey benefits from FANUC's variety of products in order to improve quality and efficiency.

FANUC Case Studies

Explore our comprehensive range of factory automation solutions, showcased in detailed case studies, and designed to optimise and streamline any manufacturing process.