ITD EOOD

FANUC Service Gives Peace of Mind

Injection moulding is usually associated with high energy costs - not so with the all-electric ROBOSHOT machines from FANUC, which have enabled ITD to achieve energy savings of 50%. In combination with an excellent service this convinced ITD to further automate with FANUC.
Success story about successful implementation o FANUC ROBOSHOT and FANUC ROBODRILL at the Bulgarian manufacturer of plastic packaging and moulds ITD Ltd. In its production ITD Ltd. is using seven machines served by FANUC CNC systems, two ROBODRILL machining centres and five ROBOSHOT plastic injection moulding machines.

Key Insights from Task to Result

Task

To guarantee its continuous production cycle, company ITD is striving to achieve maximum serviceability and trouble-free operation with all its machines.

Solution

Existing hydraulic injection moulding machines were replaced with all-electric ones. ITD’s production facilities now include five FANUC ROBOSHOT injection moulding machines with a different clamping force level. In addition, ITD deployed two FANUC ROBODRILL vertical machining centres to cover its instrument production needs.

Result

ITD has managed to reduce its production costs and has achieved a consistently high quality level. During the monitoring of energy consumption, it was established that FANUC machines provide 50% energy savings, which makes ITD's products extremely competitive.

ITD EOOD

Success story about successful implementation of FANUC ROBOSHOT and FANUC ROBODRILL at the Bulgarian manufacturer of plastic packaging and moulds ITD Ltd. In its production ITD Ltd. is using seven machines served by FANUC CNC systems, two ROBODRILL machining centres and five ROBOSHOT plastic injection moulding machines. FANUC ROBOSHOT and ROBODRILL lead to high-quality output and electricity savings of over 50%. Find out how FANUC's service ensures maximum uptime of all FANUC equipment to guarantee the continuous production cycle - 24/7.

ITD EOOD is a Bulgarian company founded in 1990 in the town of Saedinenie. ITD specialises in the production of moulds, preforms, plastic bottles, vials, caps and other types of plastic packaging. It is also engaged in recycling PET packaging, acting as a pioneer in Bulgaria in this field. The company employs about 250 people.

FIND OUT MORE ABOUT ITD

ITD Recommends FANUC's Service and Equipment for Ensuring Trouble-Free Operation

For more than 30 years, ITD has relied on FANUC Bulgaria’s maintenance services to ensure maximum serviceability and trouble-free operation with its FANUC equipment. The services used by ITD include contracts for machine servicing, maintenance, staff training and reprogramming of options to meet specific production needs.

Testimonial of ITD. Success story about successful implementation of FANUC ROBOSHOT and FANUC ROBODRILL at the Bulgarian manufacturer of plastic packaging and moulds ITD Ltd.
Testimonials quote

Ivan Daradjanski

Owner and manager of ITD.

"We have only rarely had to seek their assistance for repairs, but on those occasions, they responded quickly. We have peace of mind. We are extremely pleased and if we have to evaluate FANUC’s service, we will rate it as excellent“, said ITD’s manager.

"We have chosen FANUC because their machines help us reduce the costs required for our finished products. The ROBOSHOT injection moulding machine with CNC control is characterised by stable mechanics, reliability and easy operation, and can produce high precision casts. One of its most important benefits is its low electricity consumption – once we began working with it, it wouldn’t be long before we found out that we achieved over 50% in terms of energy savings. Compared to hydraulic machines, our production with ROBOSHOT is environmentally friendly, as there are no oils, filters or pumps, or heating from these pumps", shared Daradjanski.

Success story about successful implementation of FANUC ROBOSHOT and FANUC ROBODRILL at the Bulgarian manufacturer of plastic packaging and moulds ITD Ltd. In its production ITD Ltd. is using seven machines served by FANUC CNC systems, two ROBODRILL machining centres and five ROBOSHOT plastic injection moulding machines. FANUC ROBOSHOT and ROBODRILL lead to high-quality output and electricity savings of over 50%. Find out how FANUC's service ensures maximum uptime of all FANUC equipment to guarantee the continuous production cycle - 24/7.

"ROBODRILL, on the other hand, is a fast high-quality machine with all the options of a 4-axis machine centre. With its 24,000 revolutions, we can achieve an exceptional quality in our manufactured products at a very good price, thanks to the very low power consumption", he added.

The next stage lies in the robotisation of production both in machine-building and in the production of plastic products.

"Following market trends, the future lies in a high degree of automation, robotics and artificial intelligence. And this is what we are striving for. As a company, we rely on the loyalty to our partners when they have proven their reliability. For us, FANUC is synonymous with trust and security and we prefer to work with them.", Mr. Daradjanski concluded.

Get Inspired

FANUC Success with Robots, ROBOSHOT and ROBODRILL - Erkul Cosmetics in Turkey benefits from FANUC's variety of products in order to improve quality and efficiency.

FANUC Case Studies

Explore our comprehensive range of factory automation solutions, showcased in detailed case studies, and designed to optimise and streamline any manufacturing process.