Viskiplast

Injection Moulding Shop Shapes its Future with FANUC

There are numerous plastic injection moulding machines available on the market, but most modern manufacturers seek a core set of key attributes based on flexibility, energy efficiency and performance. As a result, the highly capable FANUC ROBOSHOT, with its potential for rapid tool changes and all-electric low energy consumption, is a proven choice for any manufacturer of plastic products looking to become more competitive and gain market share. Among those able to provide testimony is Hungary-based Viskiplast.
Success Story Video featuring Hungarian customer Viskiplast. Products shown: ROBOSHOT. Hungarian with English subtitles. Duration: 2:45

Key Insights from Task to Result

Task

Viskiplast manufactures most of its plastic parts in small volumes, typically thousands or tens of thousands. As a result, the company wanted to source an injection moulding machine with the capability to facilitate five or six rapid tool changes a day. Energy efficiency was also high on the list of desired characteristics. 

Solution

Impressed by its advanced features and energy efficiency, Viskiplast opted for a FANUC ROBOSHOT all-electric 𝛼-S100𝑖A injection moulding machine.  

Result

Viskiplast has performed its own analysis on the energy efficiency of its ROBOSHOT 𝛼-S100𝑖A, concluding that it offers a 70% reduction in energy consumption compared with a hydraulic machine. The company also highlights a number of advanced ROBOSHOT features as particularly beneficial, including automatic clamp force adjustment, and integrated mould and ejector protection. Suitably impressed, Viskiplast soon placed an order for a second ROBOSHOT machine. 

Viskiplast

Founded in 1987, Viskiplast is a second-generation family-owned specialist in plastic injection moulding. Located in Ráckeve, around 30 km south of Budapest, Hungary, Viskiplast says it has production tools and all-electric injection moulding machines that enable the most up-to-date and economical plastic component manufacturing available. Its extensive knowledge and continuous development, Viskiplast strives to provide customers with the best quality at the best price, thereby increasing its competitive edge. Furthermore, the company supports its highly skilled professional staff with continuous training and development.

FIND OUT MORE ABOUT Viskiplast
Success Story Hungarian customer Viskiplast. Products shown: ROBOSHOT.

Viskiplast Enjoys ‘Electric’ ROBOSHOT Performance

“My parents founded the company in 1987,” states Csaba Viski, Managing Director of Viskiplast. “We built a very successful injection moulding business but managed to remain a relatively small family-owned enterprise to ensure flexibility for customers. Our core business is the production of parts for roller shutters and shades, but we’re also active in a number of other fields, such as the automotive sector. In addition, we produce caps and bottle handles for the packaging industry.” 

Viskiplast makes most of its products in small volumes, with typical batch sizes in the thousands or tens of thousands.

Success Story Hungarian customer Viskiplast. Products shown: ROBOSHOT.

We perform five or six tool changes a day. So being able to work with machines that are flexible and quick to set-up is essential. That’s how we came to invest in FANUC ROBOSHOT technology.

Testimonials quote

Csaba Viski

Managing Director

In the spring of 2019, Viskiplast was invited to attend a machine demonstration at a nearby company where it could assess a number of FANUC ROBOSHOT models. Viskiplast’s delegation decided there and then that it was the type of machine required, promptly placing an order for an 𝛼-S100𝑖A model. A number of machine attributes influenced the purchase decision. 

“For a start, power consumption is far less than injection moulding machines from other manufacturers,” explains Viski. “We have since confirmed this with our own analysis: we recorded savings of 70% compared with hydraulic machines. Furthermore, the advanced functions of the FANUC ROBOSHOT, which we have not yet encountered on other machines, work very well. Automatic clamp force adjustment, for example, saves energy and puts less strain on the mould.”

Success Story Hungarian customer Viskiplast. Products shown: ROBOSHOT.

Viski also likes the ROBOSHOT’s integrated mould and ejector protection: “In our experience, mould damage or breakage cannot occur with this type of machine.” 

A few weeks ago, Viskiplast received a request for a new product required on a very short lead time.  

“Due to our existing satisfaction with FANUC, there was no question about where to go,” reports Viski. “FANUC responded very quickly to our needs and proposed several options for our consideration. We duly ordered our next ROBOSHOT machine and it will arrive in 3-4 weeks.” 

Get Inspired

FANUC Success with Robots, ROBOSHOT and ROBODRILL - Erkul Cosmetics in Turkey benefits from FANUC's variety of products in order to improve quality and efficiency.

FANUC Case Studies

Explore our comprehensive range of factory automation solutions, showcased in detailed case studies, and designed to optimise and streamline any manufacturing process.