SIMLOGIC

Robots in Dairy Production

Taking on demanding palletising tasks is child's play for robots. For complex applications, well thought-out development and design ensure production efficiency and competitiveness.
Success story of successful implementation of FANUC 410iC palletising robot at the Bulgarian dairy company ELVI by SimLogic Ltd.

Key Insights from Task to Result

Task

ELVI Ltd, a dairy products manufacturing company wanted to automate its palletising operation for yoghurt and turned to SIMLOGIC for help.  

Solution

SIMLOGIC developed solutions based on FANUC robots for the application. For the dairy producer, a FANUC M-410đť‘–C/185 four-axis industrial robot now palletises plastic crates containing yoghurt products at the end of two separate lines.  

Result

The FANUC M-410 palletises crates with a capacity of 720 crates per hour, with various palletisation options according to the operator selection.  

SIMLOGIC

SIMLOGIC Ltd is a company with vast experience in the automation of discrete and continuous production processes for various industries such as oil refining, chemical, pharmaceutical, food, metallurgy and others. The company focuses on the construction of robotic lines for palletising and materials handling and has completed a significant number of successful projects domestic and abroad.

FIND OUT MORE ABOUT SIMLOGIC
Success story of successful implementation of FANUC 410iC palletising robot at the Bulgarian dairy company ELVI by SimLogic Ltd.

Customised Palletising for Maximum Efficiency

"In order to increase their efficiency and competitiveness, Bulgarian companies are increasingly turning to the robotisation of production,” SIMLOGIC manager Plamen Penev says. “To realise such large-scale and complex projects, a strictly bespoke approach is needed for the design and development of a complete solution by specialised engineering companies such as ours." 

For the needs of ELVI Ltd, a dairy products manufacturer, SIMLOGIC designed and developed a robotic installation for palletising plastic crates containing yogurt. 

The automated line is based on a FANUC M-410 four-axis industrial robot with a load capacity of 185 kg, which palletises finished products coming from two separate lines.

Testimonials quote

Plamen Penev

Manager ELVI

ELVI developed a special gripper for picking up four crates at the same time, with its main structural elements and details designed, manufactured and assembled by their team.

The capacity of the two production lines is approximately 720 crates per hour. Importantly, the installation has the ability to palletise boxes according to operator request: from two lines on the same pallet; from one line on two pallets; or from each line on to its own corresponding pallet. 

An industrial controller provides overall system control, with an industrial touchscreen display facilitating the actual setting of parameters for palletising. The panel visuals are entirely in Bulgarian language – developed by SIMLOGIC especially for this application. As a future extension of the system, ELVI would like the industrial robot to place empty pallets in specified positions. 

Success story of successful implementation of FANUC 410iC palletising robot at the Bulgarian dairy company ELVI by SimLogic Ltd.

Get Inspired

FANUC Success with Robots, ROBOSHOT and ROBODRILL - Erkul Cosmetics in Turkey benefits from FANUC's variety of products in order to improve quality and efficiency.

FANUC Case Studies

Explore our comprehensive range of factory automation solutions, showcased in detailed case studies, and designed to optimise and streamline any manufacturing process.