Collaborative Robots FANUC > Robots > Robot finder > Collaborative Robots Menu ProductsRobotsCNCROBODRILLROBOSHOTROBOCUTIoTLaserCustomer Servicelifetime managementmaintenance servicesspare partsSolutionsIndustriesApplicationsCustomer CasesAbout FANUCCareerCountriesHistoryNews and eventsWho we areWhy FanucContact us MyFANUCDownload center Robots Robot finder LR MateLR-10 Arc weldingCollaborative Robots CR-4iACRX-5iACR-7iA and CR-7iA/LCRX-10iACRX-10iA/LCR-14iA/LCR-15iACRX-20iA/LCRX-30iACR-35iB DELTA RobotsSCARA RobotsPaint RobotsM-10M-20M-410M-710M-800M-900M-1000M-2000iAR-1000iAR-2000 Range overviewRobot accessoriesEducational packageJ-30iB controller Get Navigation Language selection follow us Sitemap Print Menu ProductsRobotsCNCROBODRILLROBOSHOTROBOCUTIoTLaserCustomer Servicelifetime managementmaintenance servicesspare partsSolutionsIndustriesApplicationsCustomer CasesAbout FANUCCareerCountriesHistoryNews and eventsWho we areWhy FanucContact us MyFANUCDownload center The future lies in the collaboration Imagine a world without safety fences, a world in which humans work side-by-side with robots. In this world, robots would execute all strenuous tasks, enabling humans to dedicate their precious time to lighter, more skilled or demanding tasks. With FANUC collaborative robots, that world has already come into existence. By integrating them into existing production environments, robots directly collaborate with humans, becoming a crucial part of the team. Alongside humans, they take over tedious, repetitive tasks, lifting up to 50 kg, thus maintaining the human’s health while automating entire assembly lines. Meet below our CR and the new CRX series. Download CR Brochure Download CRX Flyer Collaborative Robots CR-4iA Collaborative robot Axes: 6 Payload: 4 kg Reach: 550 mm CR-7iA and CR-7iA/L Collaborative robot Axes: 6 Payload: 7 kg Reach: 717 mm (CR-7iA) Reach: 911 mm (CR-7iA/L) CRX-5iA Collaborative robot Axes: 6 Payload: 5 kg Reach: 944 mm CRX-10iA Collaborative robot Axes: 6 Payload: 10 kg Reach: 1249 mm CRX-10iA/L Collaborative robot Axes: 6 Payload: 10 kg Reach: 1418 mm CR-14iA/L 6-axis robot, long arm version Axes: 6 Payload: 14 kg Reach: 911 mm CR-15iA Collaborative robot Axes: 6 Payload: 15 kg Reach: 1441 mm CRX-30iA Collaborative robot Axes: 6 Payload: 25-30 kg Reach: 1756-1889 mm CR-35iB Collaborative robot Axes: 6 Payload: 35-50 kg Reach: 1643-1831 mm CRX-20iA/L Collaborative robot Axes: 6 Payload: 20 kg Reach: 1418 mm Highlights of FANUC CRX Series Quick to install The CRX does not require any special surface to be installed and the controller is powered by a regular power source (200-240V). Space saving With only 40 kg of weight and slim design the latest collaborative robot can be quickly deployed in factories thanks to its small footprint and capabilities to be mounted anywhere (floor, upside-down and angle). With the longarm version you can even work on more confined spaces thanks to the underflip motion. Drag & Drop programming Using the Tablet Teach Pendant it is possible to do Drag & Drop programming. This functionality allows you to easily program an application in a matter of minutes. Manual Guided Teaching The CRX can easily learn from you. How? Just use the manual guided teaching function to teach the Cobot. Just lead your robot to the desired position and save it on the tablet using the drag & drop functionality. Easy to connect The new CRX offers a easy to use plugin software allowing users to install an interface for peripheral equipment easily. FANUC knows the needs of the market and provides all possible options as camera systems (iRVision), force sensor technology (FS-15ia) and much more! Great Reliability 40 years of experience building industrial robots and passion for perfection results in high reliability. FANUC is very proud to produce high quality products that will work perfectly for a long time, supporting the customers to work effectively and to increase their productivity. Highlights of FANUC CR Series Protection class IP67 The extra smooth surfaces of the CR series helps to minimise dust and dirt build up. Thanks to IP67 protection on its arm and wrist axis, it is well suited for dirty environments. Collision stop Based on a safe contact stop, FANUC CR immediately halts its current task and stops after collision with a person or a fixed object thanks to its proven sensor technology. Payload up to 50 kg The FANUC collaborative robots family can handle payloads up to 50 kg, making the CR-35iB robot the world's strongest, collaborative robot. Easy programming and handling FANUC Hand Guidance allows you to teach your collaborative robot by leading it through paths and/or use it to lift heavy objects manually. This is made possible by an emergency stop button and a three-position enabling switch that meets ISO 10218 and ISO/TS 15066. Compatible with FANUC accessories Depending on the needs, the CR robots can be equipped with a FANUC Vision Sensor, which enable them to locate or envision workpieces. Good repeatibility Despite its green exterior, the CR family operates like any other FANUC robot and is able to repeat the same movement multiple times at the exact same dexterity, leading to the automation of entire assembly operations of various industries such as of the automotive, packaging, distribution and metalworking industry. Success Stories STIHL | Handling and Shake testing of 10 kg saws To relieve their employees from heavy lifting STIHL added a CR-35iA to their production line in Waiblingen, Germany. Read more BENTELER | Loading and Unloading of testing stations At their production in Schwandorf, Germany simple tasks such as parts transportation are handled by automatic systems and thus make the work place more ergonomically. Read more Discover the wide range of collaborative opportunities Automotive machining and assembly Preventing the risk of repetitive strain injuries amongst assembly line workers, the CR series will lift and position heavy components on machining and assembly lines. The repeatability offered by using a collaborative robot for these processes also improves quality and reduces cycle times. Machine tending and part inspection The CR series is ideally suited to those machine tending applications that frequently require an operator’s presence. Eliminating the need for an additional workstation, the robots can also carry out quality control checks as part of the handling process. Picking, packaging and palletising On packaging and palletising lines, the CR series can be used to carry out dull, repetitive, dirty and dangerous handling tasks, freeing up staff to perform more complex and diversified jobs requiring human skills. Dispensing Whether they are used to apply sealants, adhesives, paints or other fluids, the CR series works safely next to humans across a range of industries. How can we help you increase your productivity? Our specialists are looking forward to supporting you. Contact us
Quick to install The CRX does not require any special surface to be installed and the controller is powered by a regular power source (200-240V).
Space saving With only 40 kg of weight and slim design the latest collaborative robot can be quickly deployed in factories thanks to its small footprint and capabilities to be mounted anywhere (floor, upside-down and angle). With the longarm version you can even work on more confined spaces thanks to the underflip motion.
Drag & Drop programming Using the Tablet Teach Pendant it is possible to do Drag & Drop programming. This functionality allows you to easily program an application in a matter of minutes.
Manual Guided Teaching The CRX can easily learn from you. How? Just use the manual guided teaching function to teach the Cobot. Just lead your robot to the desired position and save it on the tablet using the drag & drop functionality.
Easy to connect The new CRX offers a easy to use plugin software allowing users to install an interface for peripheral equipment easily. FANUC knows the needs of the market and provides all possible options as camera systems (iRVision), force sensor technology (FS-15ia) and much more!
Great Reliability 40 years of experience building industrial robots and passion for perfection results in high reliability. FANUC is very proud to produce high quality products that will work perfectly for a long time, supporting the customers to work effectively and to increase their productivity.
Protection class IP67 The extra smooth surfaces of the CR series helps to minimise dust and dirt build up. Thanks to IP67 protection on its arm and wrist axis, it is well suited for dirty environments.
Collision stop Based on a safe contact stop, FANUC CR immediately halts its current task and stops after collision with a person or a fixed object thanks to its proven sensor technology.
Payload up to 50 kg The FANUC collaborative robots family can handle payloads up to 50 kg, making the CR-35iB robot the world's strongest, collaborative robot.
Easy programming and handling FANUC Hand Guidance allows you to teach your collaborative robot by leading it through paths and/or use it to lift heavy objects manually. This is made possible by an emergency stop button and a three-position enabling switch that meets ISO 10218 and ISO/TS 15066.
Compatible with FANUC accessories Depending on the needs, the CR robots can be equipped with a FANUC Vision Sensor, which enable them to locate or envision workpieces.
Good repeatibility Despite its green exterior, the CR family operates like any other FANUC robot and is able to repeat the same movement multiple times at the exact same dexterity, leading to the automation of entire assembly operations of various industries such as of the automotive, packaging, distribution and metalworking industry.