Gnutti

Fully Automated Production of Parts, From Cassette to Cassette

Unsupervised production and easy remote management is the dream of many manufacturing companies. Gnutti Transfer took on the challenge of creating a highly automated production unit with a flexible unit architecture.
Success story about successful implementation of FANUC robots and CNC controls at the company Gnutti. The system incorporates various machines, central to which is flexible transfer to 10 stations and five robots - FANUC M-20iA/20M, M-10iA/10MS and M-10iA/10M models – that automate all phases of the process. Control is via two FANUC 30i-B Plus units.

Key Insights from Task to Result

Task

The implementation of an IoT production system that would incorporate all phases of work required to make die-cast aluminium enclosures. 

Solution

The installation integrates various machines, including flexible transfer to 10 stations and five robots involved in automating all phases of the process. Control is via two FANUC 30𝑖-B Plus NC units. 

Result

The system designed by Gnutti Transfer enables the customer to produce parts from cassette to cassette fully automatically and safely. 

Gnutti

In 1955, Quirino Gnutti established Gnutti Transfer in Brescia for the construction of lathes and transfer machines. Over the years, the business has grown and evolved, integrating new flexible, modular and innovative concepts, while paying particular attention to machine design and production sustainability. Every year, Gnutti Transfer dispatches 35-40 machines from its Ospitaletto facility.

FIND OUT MORE ABOUT GNUTTI
Image related to the success story Gnutti. FANUC Italy.

Collaboration between Gnutti and FANUC has been ongoing for 21 years and has seen the two companies combine their respective skills to implement large-scale projects and technical solutions. The system incorporates various machines, central to which is flexible transfer to 10 stations and five robots - FANUC M-20iA/20M, M-10iA/10MS and M-10iA/10M models – that automate all phases of the process. Control is via two FANUC 30i-B Plus NC units.

Fully Automated Production of Parts

Every workshop dreams of fully vertical, automated and integrated parts production, ensuring maximum reliability and flexibility, together with the potential for remote supervision and control of the entire process. Thanks to the skill and experience of Gnutti Transfer the dream has become reality.  

The project was highly complex, as Gnutti Transfer's Sales Area Manager, Giovanni Gualco explains: “The customer’s objective was to begin with raw parts in a cassette and end with finished parts back in the cassette in a single cycle.” 

                             

Success story about successful implementation of FANUC robots and CNC controls at the company Gnutti.

At the start of the process, loading is via the automatic recognition, division and control of cassette parts, before each component passes through a control station for laser marking. The transfer machine then performs machining operations prior to extraction for washing. After washing to remove any residue, the system returns parts to the cassette.  

Robots are present at all stages: a robot equipped with a vision system removes raw parts from the cassette and places them on a conveyor belt that feeds the laser machine for marking; a second robot then loads the components into the transfer machine before a third robot unloads the machine and places the parts in an intermediate station. A fourth robot loads the components into the washer; and finally, a fifth robot takes the parts from the washer and places them back in the cassette, ready for automatic relay to assembly. 

          

Success story about successful implementation of FANUC robots and CNC controls at the company Gnutti. The system incorporates various machines, central to which is flexible transfer to 10 stations and five robots - FANUC M-20iA/20M, M-10iA/10MS and M-10iA/10M models – that automate all phases of the process. Control is via two FANUC 30i-B Plus units.

The transfer machine is part of Gnutti Transfer's GR-MR flexible transfer range. It consists of 10 stations with 11 operating units mounted on a crossbar and comprises 45 axes controlled in a single process, with a cycle time of barely 8 seconds. All 33 linear axes and 10 rotating axes are equipped with FANUC motorisation featuring digital drives and fibre optic connections.  

The complexity of the project and high number of controlled axes required a huge investment in time and human resource. Involving a strategic partner like FANUC has essentially been the key to a winning technological contribution. “Strategic because FANUC is the only company able to support us in project as complex as this; winning because FANUC's technology delivers perfect system functionality,” states Giovanni Gualco. 

Giovanni Gualco

"We chose FANUC for their expertise, support and technology, FANUC is the only supplier with the expertise necessary to help us achieve this result."

Testimonials quote

Giovanni Gualco

Sales Area Manager Gnutti Transfer

The unit is Industry 4.0-certified: the chucks and all parts are fitted with sensors that analyse the data relating to the unit's functionality. An industrial PC is completely dedicated to managing the machine and controlling more than 12,000 variables, which enables the customisation of functionality that ranges from preventive/predictive maintenance to regulating process parameters. The customer can log in remotely, supervise the machine, start cycles and amend the entire system’s configuration to execute various types of processing. 

 

Get Inspired

FANUC Success with Robots, ROBOSHOT and ROBODRILL - Erkul Cosmetics in Turkey benefits from FANUC's variety of products in order to improve quality and efficiency.

FANUC Case Studies

Explore our comprehensive range of factory automation solutions, showcased in detailed case studies, and designed to optimise and streamline any manufacturing process.