The latest addition to the series of Faimond, which already has 27 patents, is the Astra cutting diamond machine, which allows us to create facets on the surface of spherical objects and holes. It is equipped with a numerical FANUC controller.
"We've known FANUC for a long time. It's a name that ensures quality and reliability", says Gianluigi Dal Lago. "Until now, we had never used their technology, but now, customers continue to require more and more complex processing methods and being able to count on a partner likeFANUC has become very important to us".
The first collaboration between Faimond and FANUC led to the implementation of a special FT-Series machine, a transfer with 4 multiple heads custom built and highly productive.
A partnership based on the common desire to win the challenges: in a few months, the project became reality and the machine started operating smoothly and without any issues. After this, a work area was developed for the molding and quality check of the pieces (the objects are loaded by the anthropomorphic robot, coined and measured, as well as they are 61 selected or discarded via a visual inspection). All with the FANUC Brand.