Začnite z iskanjem

Nizozemski proizvajalec natančnih izdelkov uporablja stroj Robodrill za obdelavo delov z izjemno natančnostjo

Naloga:

Nizozemsko specializirano podjetje za izdelavo ležajev PM Bearings je potrebovalo center za strojno obdelavo, ki z nano premiki omogoča izdelavo drobnih izjemno natančnih linearnih ležajev.

Rešitev:
Uporaba stroja FANUC Robodrill za izdelavo drobnih linearnih ležajev za medicinske, vojaške in polprevodniške aplikacije z veliko natančnostjo. Ta stroj ponuja izjemno ponovljivo natančnost ter najkrajše čase rezkanja, vrtanja, rezanja navojev in zamenjave orodij na tržišču.

Rezultat:
Podjetje PM Bearings izdeluje vse ležaje v centrih za strojno obdelavo Robodrill in ni še nikoli prekinilo proizvodnje zaradi okvare ali napake. Eden od strojev je star 19 let in še vedno deluje brezhibno. Natančnost teh strojev je neprekosljiva ne glede na to, kateri material obdelujejo.


Nano precision whatever the material

It changes over incredibly quickly from drill to tap to mill. We always have high speed spindles installed.

Robodrill produces most accurate linear bearings in the world

PM-Bearings in the Dutch Dedemsvaart specializes in ultra-precise linear guides, nano-positioning systems and complete machines, in which a micrometer-precise positioning is an absolute requirement.. The metal-working company very conscientiously chose Robodrill for producing its smallest linear bearings for medical, military and semiconductor applications.

Global player

PM-Bearings is part of the PM Group. With its Dutch offices in Dedemsvaart, Almere and Hengelo, the Group designs, develops and manufactures mechatronic systems, precision structures in sheet metal, advanced coatings and high quality solutions for the aviation and military sector. Companies all over the world call on the expertise of this Group. Almost 90 percent of the production is destined for export within Europe, to North America and Asia.

Production of linear bearings

For over 20 years, FANUC Robodrills have been assuring the production of the smallest guides in small to medium sized series of 10 to 500 pieces. The production takes place in the material that is most suited for your application, such as stainless steel, aluminium, carbon and even ceramic. You will find the bearings in, among others, semi-conductors and lithography machines for producing electronic chips, pick & place systems, microscopes and all kinds of high technology medical equipment.

Ultra-fast milling, drilling and tapping

Production Manager Pim Lüth: "We chose FANUC at that time because the Robodrills excelled in speed. And they still do that even now. Drill holes, tap threads and bevel bearings and mill to length: no other machine mills, drills and taps so fast. It changes over incredibly quickly from drill to tap to mill. We always have high speed spindles installed. In our models, we get 20,000 revolutions per minute.

Precise to the micrometer

"The precision and therefore the quality of our guides also increased significantly. Precision is vitally important for us. Our profiles deviate by maximum 2 micrometers per meter. The end product must also be finished precise to the micrometer. The maximum deviation of our bearings is 4 micrometers.

Fourth axis

PM-Bearings currently uses seven Robodrills: one a-T10B, two a-T14iAL’s, one a–T14iBL, one a-T21iDL and two six years old a–T21iEL’s. The company equipped four out of these with a fourth axis. Pim Lüth: "We had to machine our guides along all sides. The Robodrills with a fourth shaft and the DDR turntable do that in one clamping and do it faster. We use them to produce the medium sized series. On the machines with three axes, an operator must still change the piece from the side a few times."

Years of reliability

"The robustness of the machine is also a great plus. We have never yet had to interrupt our production on any of our Robodrills due to any malfunction or defect. The older Robodrill that we have, the a-T10B, is already 19 years old. It is still working perfectly."

Polyvalent control

Are there any other advantages that the Robodrill offers PM-Bearings? Pim Lüth: "You install even raft components from other manufacturers on the Robodrill. The CNC controller easily communicates with them. Due to the automation we could also reduce the cost price of our products,

Complete automation

PM Bearings has plans to fully automate the production of its high precision linear bearings within a few years. "Our goal is fully automated production. A first step in this is to fit Robodrills with the automatically opening doors and FANUIC robots to load and unload them.

Uporaba izdelkov FANUC